3 Phase Delta/Wye Calculator
Three phase power is typically delivered in two different forms, the Delta and Wye (Star) configurations. Both get their names from the physical characteristics of the configuration and the Greek letters that they resemble. The Delta configuration features a high starting torque and a inherent fault tolerance as an open element will not affect the others (although the phase current will be higher). The Wye configuration uses less starting current and is typically used for power transmission. It also uses a fourth wire.