Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
LTC3895-Slide5

Shown here is a typical 3895 schematic which produces a 12V output from a 7V to 140V input voltage range. Note that when the input voltage is below 12V the output voltage will follow the input voltage since it would be running at 100% duty cycle with the top MOSFET on continuously.

PTM Published on: 2016-07-06